Technical FAQs

Ask a Question

Where do I find CAD drawing for Lexium 28 BCH2 motors?

The CAD files for Lexium 28 are hosted for Schneider Electric by

Navigate to > Catalogs > Catalogs List and then "S" for Schneider Electric.
Choose Schneider Electric "Automation and Control"

In the "Title" pull-down select the BCH2 motor frame size you are looking for and then use the "Part Number" pull-down to choose an appropriate model.

Note that all models are not provided because the physical dimensions of the motor are not influenced by things such as, rotor inertia and winding type.
So if a model is not found, select a similar model with slightly different electrical characteristics.
Was this helpful?
What can we do to improve the information ?