Technical FAQs

Ask a Question

Configuring Concept I/O Scanning for ZBRN1 Receiver

After setting the IP address
Set the UNIT ID to 255
Read Ref Slave to 400001
Read Length to 4    (This will read 4 16 bit registers)
Read Ref Master to a location on the PLC ex. 400100

This will write to 400100, 400101, 400102 & 400103
Was this helpful?
What can we do to improve the information ?