Technical FAQs

Ask a Question

Can the M580 PAC be connected to a Gigabit Autonegotiate Ethernet switch

Title
M580 PAC Autonegotiate Ethernet switch Connection
 
Issue
M580 PAC Autonegotiate Ethernet switch Connection
 
Product Line
Applicable product lines.
 
Environment
Ethernet
 
Cause
N/A
 
Resolution
No, the M580 PAC needs to be connected to a 10/100 autonegotiate capable Ethernet switch
Was this helpful?
What can we do to improve the information ?