Technical FAQs

Ask a Question

What Operating Systems does the ProWORX 32 v2.1 SP2 Server package support?

ProWORX 32 v2.1 SP2 Server package is qualified to run on the following Operating Systems:
-----Windows NT (v4.0 SP6a or higher)
-----Windows 2000 (SP3 or higher)
-----Windows XP Professional (not home)
-----Windows Vista 32 Bit Business Edition
-----Windows 7 Pro (32-bit & 64-bit)
Was this helpful?
What can we do to improve the information ?