Technical FAQs

Ask a Question

What Operating Systems does the ProWORX 32 Client v2.1 Service Pack 2 programming software support?

The ProWORX 32 v2.1 SP2 Client package is qualified to run on the following Operating Systems:
-----Windows 98
-----Windows NT (v4.0 SP6a or higher)
-----Windows 2000 (SP3 or higher)
-----Windows XP Professional (not home)
-----Windows Vista 32 Bit Business Edition
-----Windows 7 Pro (32-bit & 64-bit)
Was this helpful?
What can we do to improve the information ?