Technical FAQs

Ask a Question

Why aren't changes made to COM'X 510 custom devices taking place?

When a change is made to a custom model it is not reflected in system devices that have been added with that custom model.

Product Line
COM'X 510

Custom Models

When a device is added to the COM'X system, it takes the properties of the device model at the time of when the device is added. Any changes to the model do not effect devices that have already been added with that model. 

*Warning: Take backups of configuration prior to modifying the device.*

To make changes to a custom device that is already added:
1) Delete the existing device.
2) Modify the existing custom model
3) Add the device to the system with the new custom model.
Was this helpful?
What can we do to improve the information ?