Technical FAQs

Ask a Question

What type of modules use the Expert Channels in M580 system ?

Title
M580 Expert Channel Modules
 
Issue
Identfying M580 Expert Channel modules
 
Product Line
M580 PAC
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 The intelligent/special purpose modules are the modules that use the Expert Channels in M580 system.
Attached below is a screenshot from the Unity Help file that explains which module are considered intelligent/special purpose modules.
Was this helpful?
What can we do to improve the information ?