Technical FAQs

Ask a Question

Which TCP port does XIP use for connection to the Premium PLC?

Issue:
Which TCP port does XIP uses for connection to the Premium PLC?

Product Line:
Premium, XIP, port number, 

Environment:
NA

Cause:
NA

Resolution:
XIP uses port 502 for connections.
 
Was this helpful?
What can we do to improve the information ?