Technical FAQs

Ask a Question

Are there any ports that need to be opened in Windows firewall in order for the Trends feature in Power Monitoring Expert 8.0 to work properly?

Issue:
The Power Monitoring Expert 8.0 Installation Guide lists port 80 is required for Diagrams, Reports and Internet access to work correctly. It doesn't list any port requirement for the Trends application to work correctly. 

Product Line:
Power Monitoring Expert 8.0

Environment:
Power Monitoring Expert Software Configuration

Cause:
The Trends Application does a call to IIS so a port needs to be open in order for it to work correctly. 

Resolution:
There needs to be no additional port other than port 80 open in order for Trends application to work correctly. The Trends application uses a standard HTTP call to TrendsWebService via IIS. So, if one can load the Trends application, one should be able to get to TrendsWebService.
Was this helpful?
What can we do to improve the information ?