Technical FAQs

Ask a Question

Osisense XC - What is the ZCY22S46 roller head ?

In the adapted ZCY22S46 ceramic roller head, there is only one different part with the standard ZCY22 roller lever, the ceramic roller lever is 20mm longer, by an additional part (total length 80mm instead of 60mm). See attached drawing. 2015 logistic situation : available to order through our international distribution center in France, product in stock.

Was this helpful?
What can we do to improve the information ?