Technical FAQs

Ask a Question

Preventa - Technical difference between XZCP29P12L10 and XZCP29P11L10 pre-wired M12 8-pin connectors

Attached corresponding datasheets.
Please note that the pre-wired M12 8-pin connectors are used in the Preventa safety components, for the same function :
- XZCP29P12L* in the XCSDM3/4 magnetic systems,
- XZCP29P11L* in the XUSL4E-2E light curtains.

Differences : wire colors and pin-out (attached). Both products have encoding A.
User-added image
Was this helpful?
What can we do to improve the information ?