Technical FAQs

Ask a Question

What is the difference between iRIO with USB port and without USB port ,any impact?

There is not difference between iRIO with USB port and without USB port, USB ports are never used on the iRIO and the design has been modified and does not have any impact
Was this helpful?
What can we do to improve the information ?