Technical FAQs

Ask a Question

What is the input voltage requirements for the Quantum 140CPS12400 power supply?

Issue:
What is the input voltage requirements for the Quantum 140CPS12400 power supply?

Product Line:
Quantum, power supply

Environment:


Cause:


Resolution:
An input voltage of 93-138 VAC or 170-276 VAC is required for the Quantum 140CPS12400 power supply.
Was this helpful?
What can we do to improve the information ?