Technical FAQs

Ask a Question

Does the Magelis targets offer remote access via a local or wide area network?

Issue:
Does the Magelis targets offer remote access via a local or wide area network?

Product Line:
HMIGTO/GTU/STO/STU, XBTG/GC/GH/GK/GT, iPC, Compact, Smart, Flex Box, Box PC, Panel PC

Environment:


Cause:


Resolution:
With the current version of Vijeo Designer, v6.2, there are two options to remotely access the Magelis targets.  One option is Web Gate using Internet Explorer with Windows operating systems.  The other option is to use an iOS or Android app called Vijeo Design'Air which will need to be purchased.
Was this helpful?
What can we do to improve the information ?