Technical FAQs

Ask a Question

Is there a non-iPC Magelis target that could connect to a secondary monitor?

Issue:
Is there a non-iPC Magelis target that could connect to a secondary monitor?

Product Line:
HMIGTO, dual monitor, XBTGT, HMIGTU

Environment:


Cause:


Resolution:
No, we do not offer any non-iPC Magelis targets with the option to connect to a secondary monitor.
Was this helpful?
What can we do to improve the information ?