Technical FAQs

Ask a Question

How to Edit the Percentage of an Apportioned Device in Hierarchy Manager

An apportioned device (meter) can be created when adding a device to a hierarchy node. There is a percentage text box field in the device selection dialog. This text box defaults to 100%, and leaving the value at 100% adds the device to the node. This value can be changed to anything other than 100% to create an apportioned meter.

Product Line
Power Monitoring Expert (PME)

Hierarchy Manager

To create an apportioned device after the device was added.

The percentage for an apportioned device cannot be edited once it is set. To change the percentage, delete the device from the hierarchy and add it again as a new entry with the required percentage.
Was this helpful?
What can we do to improve the information ?