Technical FAQs

Ask a Question

Which software tool do I need to load the firmware to a Unity Controller?

Unity Loader is use to load the firmware for the M340, M580 and Momentum Unity controllers.

The OS Loader is use to load the firmware in the Quantum and Premium Unity controllers

Note. The Unity Loader is a seperate tool that is not included with Unity Pro.
Was this helpful?
What can we do to improve the information ?