Technical FAQs

Ask a Question

How do you fix the ProWORX 32 network page titles that are incorrectly displayed in the Network Navigation window?

There is a way to correctly offset the network names in ProWORX 32. The easiest way to do this would be to first export the database as a XLS file. Open the XLS file in Excel and open the page for networks. Under the Network Heading you can cut/paste the network names so they line up correctly. Save the XLS file in Excel and then import the file back into ProWORX 32 using the Overlay option. Close the Network Navigator window then reopen it and the correct network name changes should be there.
Was this helpful?
What can we do to improve the information ?