Technical FAQs

Ask a Question

Which power supply is recommended to be used with the HMIGTU Terminals?

Branch Circuit Protective device shall be used for rating 20A for 12 to 24Vdc input device on
the models EXCEPT for HMIDT351.

- You must use DC input with an isolating source for the models except for HMIDT351.
- You must use DC input with a Class 2 power supply for HMIDT351.
Was this helpful?
What can we do to improve the information ?