Technical FAQs

Ask a Question

Quantum 140NOE77101 cannot display webpage using Java version 1.8

Quantum 140NOE77101 v6.5 Firmware Upgrade will resolves the Java v1.8 webpage display issue.
Please see attachments for Unity and Non Unity.

----------------------------------------------------------------------------------------
Below is the 140NOE77101 6.5 Executive for Unity OSloader.
----------------------------------------------------------------------------------------
General Quantum Ethernet Module Upgrade Procedure
----------------------------------------------------------------------------------------    
    
Pre-conditions:    
1. The CPU module must be in STOP mode and the NOE must have NO TCP traffic.     
2. A loss of power during the upgrade may cause a NOE module to be inoperable. Make sure the power supply on the NOE rack will not be interrupted during the upgrade.    

For Unity Pro User  (Unity OS Loader)    
1. Verify the kernel and Exec using Unity OS Loader. Refer to the NOE Exec. Sheet for checking the right version.    
2. Get and extract the exec and web page combined file to a directory on the PC    
3. Using the Unity OS loader download the exec and web pages to the NOE module.    

-------------------------------------------------------------------------------------------------
Below are the 140NOE77101 6.5 Executive files for Non-Unity User.
-------------------------------------------------------------------------------------------------
General Quantum Ethernet Module Upgrade Procedure
-------------------------------------------------------------------------------------------------        
        
Pre-conditions:        
1. The CPU module must be in STOP mode and the NOE must have NO TCP traffic.         
2. A loss of power during the upgrade may cause a NOE module to be inoperable. Make sure the power supply on the NOE rack will not be interrupted during the upgrade.        
        
For Concept /  Proworx User         
Exec Upgrade Procedure ( Exec Loader utility):        
1. Verify the kernel and Exec using  Exec Loader. Refer to the NOE Exec. Sheet for checking the right version.        
2. Get and extract the exec file to a directory on the PC        
3. Using the  Exec loader download the exec to the NOE module.        
        
Web Site Upgrade Procedure:    
*** Use FTP script upgrade ***         
1. Complete Exec Upgrade using  Exec Loader.        
2. Extract files from web page zip file to a empty directory on the PC.        
3. Open a command line (MsDos session on the PC), change to the directory containing the web files.        
4. Run the command "put771 a.b.c.d" where a.b.c.d is the IP address of the NOE module to be upgraded. For example: "put 771 192.168.1.1" to upgrade a NOE module at address 192.168.1.1        
5. Follow the instruction presented on the screen to finish the ftp upgrade        


 
Was this helpful?
What can we do to improve the information ?