Technical FAQs

Ask a Question

Is the Twido PLC line being phased out and going to be obsoleted?

The Twido line of PLC products is being discontinued. The end of commercialization date is 12/31/2016.
Impacted Catalog Numbers are: TWDLCAA10DRF, TWDLCAA16DRF, TWDLCAA24DRF, TWDLCAA40DRF, TWDLCAE40DRF, TWDLCDA10DRF, TWDLCDA16DRF, TWDLCDA24DRF, TWDLCDA40DRF, TWDLCDE40DRF, TWDLMDA20DRT, TWDLMDA20DTK, TWDLMDA20DUK, TWDLMDA40DTK, TWDLMDA40DUK,

The newer Modicon M221 and M241 offer is the appropriate replacement.
Was this helpful?
What can we do to improve the information ?