Technical FAQs

Ask a Question

How do I access the One Line Documentation window in the ProWORX 32 software?

To access the One Line Documentation window click the "1 Line..." button at the top right corner of the Documentation editor

- or -

Follow these four steps:

1 - Right-click your project.

2 - Click properties.

3 - Click the Documentation tab.

4 - Select the Display One Line Documentation Window check box.

To turn off the One Line Documentation window:

Click the "Edit..." button at the top right corner of the Documentation Editor

- or -

Clear the Display One Line Documentation Window check box in step 4 above.

Was this helpful?
What can we do to improve the information ?