Technical FAQs

Ask a Question

Preventa XCS - Wiring diagram of the solution 2 XCSDMC790* magnetic switches and XPSAF5130(P) unit

Find attached the requested diagram with the safety level information. Alternative solution to reach PLe category 4 consists of 2 switches XCSDM*5* + XPSDMB unit, even if both switches have a LED. Be careful technically the XPSAF5130(P) unit can monitored only 1 XCSDM*7* with LED.
Was this helpful?
What can we do to improve the information ?