Technical FAQs

Ask a Question

The time stamp of the alarm in the Magelis Alarm Summary object is not correct, what could be the issue?

Issue:
The time stamp of the alarm in the Magelis Alarm Summary object is not correct, what could be the issue?

Product Line:
Magelis XBTGC/GH/GK/GT, HMIGTO/GTU/STO/STU, iPC, Box PC, Panel PC, Alarm, clock, time stamp

Environment:


Cause:


Resolution:
The Alarm takes it's time from the Magelis system clock.  If the system clock is not in the same time zone or clock is off, then the time stamp on the Alarm will be incorrect.
Was this helpful?
What can we do to improve the information ?