Technical FAQs

Ask a Question

What is the Schneider Electric reference number for the Berger Lahr RSM41/ 8 NDG 24 50/60

The Berger Lahr  RSM41/ 8 NDG   24 50/60 is a legacy product and can only be order through select distributors and only if needed as spares to replace existing RSM41/ 8 NDG   24 50/60 motors.
There is also a 25 piece minimum order on the RSM41/ 8 NDG   24 50/60

The reference number for ordering RSM41/ 8 NDG   24 50/60 is  0011052003000
Was this helpful?
What can we do to improve the information ?