Technical FAQs

Ask a Question

Why doesn't Vijeo Design'Air work on the newly updated IOS version?

Typically when Apple updates the Operating System on their iDevices from say version X to Version X+1, the Vijeo Design'Air app will fail to launch on the updated IOS version. The reason for this is because the app needs to be recompiled an updated Software Development Kit by R&D and a update needs to be published to Apple App Store once it is available. Typically the updated app will be published only after the new IOS OS is released. The time to have the updated app publish is dependant on Apple, as they must review the app and approve it. This typically takes anywhere from 1 -3 weeks after the new IOS version is released.
Was this helpful?
What can we do to improve the information ?