Technical FAQs

Ask a Question

How come the Magelis HMIG5U will not wake up from sleep?

Issue:
How come the Magelis HMIG5U will not wake up from sleep?

Product Line:
HMIG5U, sleep, hibernation

Environment:


Cause:


Resolution:
When you set the HMIG5U power settings to Balance power.  You will enable the Windows hibernation sleep. Due to the HMIG5U does not have power button, therefore, not able to recover from hibernation.  To disable hibernation, go to Control Panel -> Power Options, for the Balanced plan select "Change plan settings" then select "Change advanced power settings".  Under sleep there is a field for "Hibernation After" change the value from 360 to 0.  This change will not put the target into hibernation.  

Make sure the EWF is disable when changing the Windows system settings.
Was this helpful?
What can we do to improve the information ?