Technical FAQs

Ask a Question

Does the M340 meet the requirements for ANSI C37.90.2 ?

Title
M340 and the requirements for ANSI C37.90.2
 
Issue
M340 and the requirements for ANSI C37.90.2
 
Product Line
M340
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
Unfortunately, we do not test to the ANSI C37.90.2  standard.Therefore the M340 does not meet the requirements for ANSI C37.90.2.
Was this helpful?
What can we do to improve the information ?