Technical FAQs

Ask a Question

How to allow EM4800 to upload onboard data to SPM or PME

Issue:
EM4800 doesn't upload onboard data when data gaps occur

Product Line:
EM4800
Struxureware Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x, 8.0

Environment:
Struxureware Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x, 8.0
EM4800

Cause:
EM4800 firmware older than rev 1.46 does not support the SE driver and will not upload onboard data.

Resolution:
Upload the EM4800's firmware to version 1.46 or newer to use the SE device type in SPM/PME and allow for onboard uploads. 
Was this helpful?
What can we do to improve the information ?