Technical FAQs

Ask a Question

Preventa XCS - Datasheet of the XCSDMP790L01SB6 magnetic switch

Please find attached the datasheet of the XCSDMP790L01SB6 adapted switch, using a special connector M12 pin-out :
- first contact between pins 1-2,
- second contact between pins 3-4.
It is not shown into the Preventa XCS catalogue. It cannot be replaced by the standard XCSDMP790L01M12 magnetic switch.
Logistic situation in 2016 : available to order without any customer restriction, product not in stock (manufactured at order reception).
Was this helpful?
What can we do to improve the information ?