Technical FAQs

Ask a Question

Firmwares SV3.30 of Quantum CPU Low End are removed from shopping kiosk and !

We have decided to remove those firmwares because of an issue seen on 140CPU31110 ( management of memory protection is common to all Low End CPUs): Setting memory protect switch to on makes Run led is switched off even if CPU is still in run, possibly leading to confusion . A SV 3.31 , containing the fix, is now published .
Was this helpful?
What can we do to improve the information ?