Technical FAQs

Ask a Question

EM4800 TR3 Report Record Types

Issue
The EM4800 TR3 report does not say what type of measurements it is recording

Product Line
EM4800 

Environment
Published Reports on the EM4800 FTP

Cause
The TR3 reports number the type of measurement, but does not indicate what the number indicates

Resolution
Type   Format Record Description
0    Comments F/W and Model Number Information
1    Int32 Wh Interval Wh (Del – Rcv) per meter per interval on meter
2    Int32 Wh Cumulative Wh register per meter (Del – Rcv) 
  Events  Internal use only
  Unused  
  Unused  
  Reserved  
7   Float Voltage Instantaneous voltage of phase 
8 Float Current Instantaneous current associated with each probe
9   Int32 Active Power Average Watt hours per probe per interval
10    Reserved  
11 Int32  Apparent Power Average VA hours per probe per interval
12    Reserved  
13    Reserved  
14    Reserved  
15   Float  Pulse Count Interval Pulse count x scale factor per pulse input per interval
16    Int32 Low Phase Binary coded output 1=phase Pn-1, 2=phase Pn-2,
4=phase Pn-3 has been 0 for the last 24 hrs.
17    Reserved  
18    Reserved  
19    Reserved  
20    Reserved  
21    Reserved  
22    Reserved  
23  Float  Phase 1 Voltage Voltage for element 1 of meter N
24    Float Phase 2 Voltage Voltage for element 2 of meter N
25 Float Phase 3 Voltage Voltage for element 3 of meter N
26   Meter ID Per meter point meter names programmed 
27   NA  
28 Int32 Wh Interval Rcv Wh received per meter per interval
29 Int32 VARh Interval Del VARh delivered per meter per interval
30  Int32 VARh Interval Rcv VARh received per meter per interval
31 Int32 VAh Interval Vah per meter per interval
32   NA  
33 Int32 Wh Register Rcv Wh received per meter cumulative
34 Int32 VARh Register Del VARh delivered per meter cumulative
35 Int32 VARh Register Rcv VARh received per meter cumulative
36 Int32  VAh Register Vah per meter cumulative
37   NA  
38 Float Pulse Count Register Pulse count x scale factor per pulse input cumulative
39 Badge Numbers Per meter point Per meter point badge numbers programmed into
meter
40 Float Peak Current 1 Peak current per interval for element 1 of meter N
41   Float Peak Current 2 Peak current per interval for element 2 of meter N
42 Float Peak Current 3  Peak current per interval for element 3 of meter N
43 Int32 Peak Demand Peak Demand and TS Per meter point, reported once per TR3 file
44 Int32 Present Demand  Demand per meter point per programmed demand interval in watts


Note: Not all record types are available on the EM4800
Was this helpful?
What can we do to improve the information ?