Technical FAQs

Ask a Question

Preventa XU - Wiring diagram of the association XUSL4E-2E light curtain with the XPSMCMER0002 expansion unit

Please find attached the wiring diagrams of the association XUSL4E-2E light curtain with the XPSMCMER0002 expansion unit in 22.5 mm wide.
Such unit can be used to supply contactors in AC supply different from the 24Vdc, or to increase the breaking capacity of the curtain OSSD's.
Was this helpful?
What can we do to improve the information ?