Technical FAQs

Ask a Question

Osisense XC - What is specific for ZCKJ5H49 ?

H49 prefix in XCKJ series is a specification for Sweden. It means special "positive opening operation" marking on the front cover, requested in the past by Sweden for ZCKJ5H49 & ZCKJ7H49 ref (see attachement). Please note that the european positive opening (arrow in the circle) exists on the switch body side, which is compliant to the current standards.
Our position : In 2015, replace the obsolete ZCKJ7H49 reference with obsolete marking by the standard ZCKJ7 with current "positive opening operation" marking. The ZCKJ5H49 reference is still available to order in 2015. if the customer agrees, he can replace it by the standard ZCKJ5 contact body.
Was this helpful?
What can we do to improve the information ?