Technical FAQs

Ask a Question

Preventa XU_Alternative to the obsolete XUSLPB2A500M light curtain for body protection with passive receiver

Regarding the attached technical data of the obsolete XUSLPB2A500M or XUSLPB2A600M type 4 light curtain for body protection with passive receiver, it is possible to replace each of both references by the XUSL4E2BB051N type 4 light curtain for body protection, compatible on the sensing distance (high range selectable by wiring), the response time (better), the beam number (2). Attached XUSL4E2BB051N technical data.
Difference of technology (transmitter & receiver separated, need a transmitter supply); lower price.
Was this helpful?
What can we do to improve the information ?