Technical FAQs

Ask a Question

Is the 'Save to Flash' function available on a Hot Standby system in Concept?

No, 'Save to Flash' is not available on a Concept Quantum IEC Hot Standby system.

'Save to Flash' is also not available in the simulator.
Was this helpful?
What can we do to improve the information ?