Technical FAQs

Ask a Question

When I import a .DIF file from Excel back into ProWorx NxT, I get the error "Total descriptors must be increased"?

In ProWORX NxT, go into "Database Setup", increase the Descriptor Field Width to 15 and the Number of Descriptor Fields to 9.

Was this helpful?
What can we do to improve the information ?