Technical FAQs

Ask a Question

How can I tell if the CF card or USB flash drive in the Magelis target is bootable?

Issue:
How can I tell if the CF card or USB flash drive in the Magelis target is bootable?

Product Line:
Magelis XBTGC/GK/GT, HMIGTO/GTU/STO/STU

Environment:


Cause:


Resolution:
Below are the list of files that will make the CF card or USB flash drive downloadable to the Magelis targets (see image):
FDATA folder
PUBLIC folder
AGP.SYS
BSP.OSC
LDML.SYS
MAIN.SYS
STUP.SYS
VERSION.SYS

 
Was this helpful?
What can we do to improve the information ?