Technical FAQs

Ask a Question

How many expansion racks can you have on the M340 PLC?

The maximum M340 expansion racks allowable:
(P341000 version <= v02.00) Max. 2 XBP racks
(P3420xx version <=v 02.00) Max. 4 XBP racks
Was this helpful?
What can we do to improve the information ?