Technical FAQs

Ask a Question

What is the current part number for the Connexium Tofino firewall?

Title
Connexium Tofino Firewall 
 
Issue
Connexium Tofino Firewall part number
 
Product Line
Connexium Tofino Firewall, TCSEFEA23F3F22
 
Environment
N/A
 
Cause
N/A
 
Resolution
 The current Connexium Tofino Firewall part number is TCSEFEA23F3F22
1) This Base model includes the Modbus TCP Enforcer
2) Optional Loadable Security Modules for the ConneXium Tofino include:
a) TCSEFM0000 ConneXium Tofino OPC-LSM, which is the OPC Enforcer deep packet engine
b) TCSEFM0001 ConneXium Tofino EIP-LSM, which is the EtherNet/IP Enforcer deep packet engine
Was this helpful?
What can we do to improve the information ?