Technical FAQs

Ask a Question

Osisense XM_Specificity of the XMPR12C2231C202 pressure switch

The special XMPR12C2231C202 pressure switch is the obsolete XMPR12C2231 switch with factory settings 6.0 (PB) - 8.0 (PH) bar.
This special part number is still available to order in 2015.
Was this helpful?
What can we do to improve the information ?