Technical FAQs

Ask a Question

Osisense XM_Specificity of the XMPE12C2531C202 pressure switch

Special XMPE12C2531C202 pressure switch is the obsolete XMPE12C2531 switch with factory settings 6.0 (PB) - 8.0 (PH) bar.
This special part number is still available to order in 2017, under logistic reference XMPE12C2531C202AB.
 
Was this helpful?
What can we do to improve the information ?