Technical FAQs

Ask a Question

Preventa XCS - XCSLE252531M2 pin-out of the M23 connector

Please find attached the wiring diagram of the XCSLE252531M2 safety switch, having 1NC + 1NO main contacts and 1NC + 1NO electromagnet contacts. It is a version with locking by electromagnet on de-energisation, with M23 16-pin connector. The electromagnet contacts are represented electromagnet not energised
Was this helpful?
What can we do to improve the information ?