Technical FAQs

Ask a Question

Latest Firmware version of Com'X 200/210 and Natively supported device type in the Energy Server Com'X 200/210

Issue
A user would like to know what is the latest version of firmware and Natively supported device type in the Energy Server Com'X 200/210.
 
Product Line
COM'X200 / EBX200
COM'X210 / EBX210
 
Environment
Ethernet Gateway supported devices

Cause
It may be unclear where to obtain the list of supported device types and firmware upgrade files
 
Resolution
The latest version of firmware for Com'X 200 is 3.5.15 and the Com'X 210 is 3.5.24. Please find the firmware files below.
They can be downloaded from the following links as well.
COM'X200 firmware
COM'X210 firmware
 
In addition, review the attached PDF (DeviceList_ComX200_210_2.2.1.pdf) for the list of Natively Supported Device Types on Com'X 200/210 with Firmware Version 2.2.1.
Note: With firmware 3.5.24, the Com'X 210 also supports Masterpact MTZ and the EM4399.

For instructions on how to upgrade the firmware, view article FA270261.
Was this helpful?
What can we do to improve the information ?