Technical FAQs

Ask a Question

Is termination required on the un-used port of a MB+ Dual-Cable BM85 Unit when connecting to a single cable MB+ network?

Yes. If you are installing a dual-cable unit on a network that has only a single cable, connect the live MB+ cable to the rear panel CHANNEL A connector. Plug a Terminating Connector (Modicon part number AS-MBKT-185) into the CHANNEL B connector.
Was this helpful?
What can we do to improve the information ?