Technical FAQs

Ask a Question

Preventa XCS - XCSLF383831M3 pin-out of the M23 connector

Please find attached the wiring diagram of the XCSLF383831M3 safety switch, having 3NC main contacts and 3NC electromagnet contacts. It is a version with locking by electromagnet on de-energisation, with M23 19-pin connector. The electromagnet contacts are represented electromagnet not energised.
Was this helpful?
What can we do to improve the information ?