Technical FAQs

Ask a Question

Preventa XCS - XCSLF272531M2 pin-out of the M23 connector

Please find attached the wiring diagram of the XCSLF272531M2 safety switch, having 2NC main contacts and 1NC + 1NO electromagnet contacts. It is a version with locking by electromagnet on de-energisation, with M23 16-pin connector. The electromagnet contacts are represented electromagnet not energised.
Was this helpful?
What can we do to improve the information ?