Technical FAQs

Ask a Question

What is the part number for the connector set that can be ordered for a Lexium 32M drive?

Issue: Part number for the set of spare connectors that can be ordered for a Lexium 32 M drive.

Product Line: Lexium 32M drive.

Environment: None

Cause: Spare

Resolution: The part number for the set of connectors that can be ordered for a Lexium 32M drive is  VW3 M2 203 . It comes with 4 connectors for the line supply, 2 connectors for the I/O, 2 connectors for the motor power supply and 1 connector for the holding brake.
Was this helpful?
What can we do to improve the information ?