Technical FAQs

Ask a Question

What is the ConneXium switch Power/Alarm Contact terminal block?

Title
ConneXium switch Power/Alarm Contact terminal block
 
Issue
ConneXium switch Power/Alarm Contact terminal block part number
 
Product Line
Connexium
 
Environment
Connexium
 
Cause
N/A
 
Resolution
 We do not have any separate part number for the ConneXium switch Power/Alarm Contact terminal block.
Below is information from Phoenix Contact that has all the specs for the type of connector used on our ConneXium switches.

MSTB 2,5/ 6-ST-5,08 - Plug component, nominal current: 12 A, rated voltage: 250 V, pitch: 5.08 mm, no. of positions: 6, type of connection: Screw connection


 
Was this helpful?
What can we do to improve the information ?