Technical FAQs

Ask a Question

Can a short coaxial cable be used with 140CRP93xxx or 140CRA931xx and a 140NRP9540x?

Title
140CRP93xxx or 140CRA931xx connection to a 140NRP9540x
 
Issue
140CRP93xxx or 140CRA931xx connection to a 140NRP9540x
 
Product Line
140CRP93100, 140CRA93100, 140CRP93200, 140CRA93200, 140NRP95401, 140NRP95400
 
Environment
Remote IO (S908)
 
Cause
N/A
 
Resolution
 The coaxial cables with tap and trunk terminator between a 140 CRP 9•• ••/140 CRA 9•• •• and a 140 NRP 954 0• in the same backplane can be replaced by a short coaxial cable: The short coaxial cable is a RG-6 cable fitted with type F female connectors. The maximum length of this cable is 30 cm (11.8 in.).
NOTE: You can use the pre-assembled short coaxial RG-6 cable of the kit (reference RPXKITCRP) or prepare your own short coaxial cable,
Was this helpful?
What can we do to improve the information ?